Instant Record feature on the DX4500/DX4600 Series DVR

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

How to use the Instant Record feature on the DX4500/DX4600 Series DVR

Product Line

Pelco Video Management

Environment

DX4500/DX4600 Series

Cause

Enable Instant Record feature

Resolution

 
INSTANT RECORD SETUP
  1. On the front panel or remote control, press the up/down arrow buttons  to highlight Instant Record.  Using the mouse, click Instant
    Record
    . The Instant Record option is highlighted and the property settings appear.
     
  2. To configure a channel’s record setting for a motion event, do the following: 

    On the front panel or remote control, press ENTER. Press the left/right arrow buttons  to select the resolution, quality, and
    image rate fields, and press ENTER. Then press the up/down arrow buttons  to set the settings for a channel. Using the mouse,
    click the settings. 

    Repeat step 2a for additional channels.