How to program a Spectra III or Spectra IV to resume a pattern after a power outage?

Issue

How to program a Spectra III or Spectra IV to resume a pattern after a power outage?

Product Line

Pelco Cameras

Environment

  • Spectra Series

Cause

Programming of Park Action after a Power Outage has occurred.

Resolution

The Spectra III SE and IV SE Series (27x or higher model) feature a programming option that is referred to as Power Up Action. Power up action allows the dome to resume its prior activity or direction before the power outage occurred. Accessing the Spectras Main Menu requires Preset 95 programming option from your control system.

  1. Use the 95 preset command to access the camera main menu.
  2. Enter DOME SETTINGS menu option and then enter POWER UP.
  3. Enter POWER UP ACTION and scroll through options until PATTERN is displayed.
  4. Exit Menu.

* Option and Actions programming features for Power Up Action will vary depending on model of Spectra system and/or version using.