Why will the preset 95 camera menu not display on a new Spectra IV analog dome using a CM9760-KBD/KBR Intelligent Keyboard?

Issue

Why will the preset 95 camera menu not display on a new Spectra IV analog dome using a CM9760-KBD/KBR Intelligent Keyboard?

Product Line

Pelco Cameras, Pelco Matrix

Environment

  • Spectra Analog Series

Cause

Menu Access of Spectra for viewing settings or programming options.

Resolution

When having issues accessing the preset 95 menu on a Spectra IV analog dome, try turning on Switch 3 on SW2 located on the base of the dome. This may help with other situations/issues as well

  • AD32 switch may also be enabled. If enabled, attempt setting Preset 28