How do I set the KBD300A keyboard for P protocol at 9600 baud rate?

Issue

How do I set the KBD300A keyboard for P protocol at 9600 baud rate?

Product Line

Pelco Matrix

Environment

KBD300A keyboard

Cause

PTZ function - Dip Switch settings.

Resolution

Configure the dip switches on the keyboard as follow:

Dip switch number 5, 6, and 8 to ON.