Which models of Spectra IV domes would replace the Spectra II domes?

Issue

Which models of Spectra IV domes would replace the Spectra II domes?

Product Line

Pelco Cameras

Environment

  • Spectra II
  • Spectra IV

Cause

Models to replace discontinued Spectra II series

Resolution

There are three models of Spectra IV that  can be used to replace the Spectra II domes.

  •  Indoor in ceiling SD423-F0
  •  Indoor Pendant SD423-PG-0
  •  Environmental Pendant SD423-PG-E0