Where do I land the wires from the microphone to the AUD-1?

Issue

Where do I land the wires from the microphone to the AUD-1?

Product Line

Pelco Cameras

Environment

  • IDE20DN
  • IE Sarix
  • AUD-1 (Audio)

Cause

Enable the connection of the microphones and speakers using UTP wiring connected to the audio adapter through a terminal block.

Resolution

On the AUD-1 connect the wires as follows:
 
A is 12VDC + RED
B is MIC + BLACK
C GROUND BARE WIRE