How do I bring up the Main Menu for the Spectra Series PTZ cameras using the DX Series Client software?

Issue

How do I bring up the Main Menu for the Spectra Series PTZ cameras using the DX4100 PC Client or DX Series Client?

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • Spectra IV SE
  • DX4100 PC Client
  • DX4500/4600 PC Client
  • DX 8100 Client
  • DX Series Client

Cause

Access the Spectra menu to configure the dome settings.

Resolution

The Main Menu can be accessed by the Pgm button or calling a Preset.

Pgm button

  1. On the PTZ control panel, click the Pgm button. Use the FOCUS +/- to navigate the menu and IRIS + to select.

Using a Preset:

  1. On the toolbar, click the Live  icon.
  2. On the View menu, point to OSD, and verify the PTZ check box is selected.
  3. In the main display window, click on a camera that displays the PTZ  icon.
  4. On the PTZ control panel on the right, click the Set button then enter the number of 95 and click Preset.
  5. Use the FOCUS +/- to navigate the menu and the IRIS + to select.