How to set the Spectra IV dome positioning system for P protocol address number 1.

Issue

No communication to the Spectra IV.

Product Line

Pelco Cameras

Environment

Spectra IV

Cause

Protocol of the Spectra IV dome need to match the control systems.

Resolution

To set the Spectra IV dome for P protocol address number 1:

  1.  Turn all of the switches on SW1 to OFF