Can the TXB-N-F translator board be use in place of the TXB-N-P translator board in the Spectra IV IP?

Issue

Can the TXB-N-F translator board be use in place of the TXB-N-P translator board in the Spectra IV IP?

Product Line

Pelco Cameras

Environment

  • TXB-IP-F
  • TXB-IP-P
  • Spectra IV Series

Cause

Installation of TXB-IP-F or TXB-IP-P within compatible Spectra housing.

Resolution

No. The TXB-N-F is the IP communication module for in-ceiling back boxes and the TXB-N-P is the IP communication module for pendant back boxes.