What are the default login PIN numbers for a CM9760-KBD connected to a CM9700 Series Matrix?

Issue

What are the default login PIN numbers for a CM9760-KBD connected to a CM9700 Series Matrix?

CM9760-KBD Default PIN

Product Line

Pelco Matrix

Environment

  • CM9760-KBD-XX
  • CM9760-KBD-B-XX
  • CM9760-KBR-XX

Cause

The PIN number to log onto the CM9760 Keyboard has been forgotten or misplaced.

CM9760-KBD Default PIN

Resolution

CM9760-KBD Default PIN

1234

Will automaticly go to the next screen requesting a Monitor.

The default logon PIN numbers when assigned by System Manager when programming a CM9700 Series Matrix are:

Version 7 and version 8: 1111, 2222, 3333, etc..

Version 9: 0101, 0202, 0303, etc...