Change IP address on a DVXe MasterControl system.

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

How to enter an IP address on a DVXe MasterControl system.

Product Line

Pelco Video Management

Environment

DVXe MasterControl system

Cause

Can't access Windows in the DVXe

Resolution


This requires logging into the system with the administrator user account. 
 

  1. Right-click the Utilities icon located on the lower right portion of the taskbar.
  2. Select Setup.

     


     
  3. Locate the Network tab and select the Intel PRO/1000 PM Network Connection for the Adapter.
  4. Enter the IP Address information.
  5. Click Done, the IP Address settings will not take effect until you reboot the DVXe system.