Clear the time/date and titles display on the CM9760-MDA Master Distribution Amplifier.

NOTICE

POTENTIAL FOR DATA LOSS.
The steps detailed in the resolution of this article may result in a loss of critical data if not performed properly. Before beginning these steps, make sure all important data is backed up in the event of data loss. If you are unsure, please contact Product Support Services prior to attempting the procedure below.

Issue

How do I clear the time/date and titles display on the CM9760-MDA Master Distribution Amplifier?

Product Line

Pelco Video Management, Pelco Matrix

Environment

CM9760-MDA Master Distribution Amplifier version 2.05 or newer

Cause

Turn off Title/Time/Date text display on all channels.

Resolution

To clear the time/data titling overlay from the CM9760-MDA Master Distribution Amplifier video outputs perform the following steps:

1. Unplug the CM9760-MDA power cord.

2. Set the MDA to unit ID 33:

     a. Set DIP switches 1, 2, 3, 4, 5, 7 and 8 to the OFF/UP position

     b. Set DIP switch 6 to the ON/DOWN position.

3. Plug in the CM9760-MDA power cord.

4. A 30-second timer starts - before the 30 seconds elapses (18-20 seconds has proven to be effective), set DIP switch 6 to the OFF/UP position.

After 30 seconds have elapsed, the CM9760-MDA checks whether the unit ID is different from the initial setting of 33. If the unit ID has changed, the CM9760-MDA title/time/date text display is cleared.

Note:  The DIP Switch is located on the back of the CM9760-MDA.

  • OFF = UP
  • ON = DOWN