Hard drive upgrade/replacement options for DX8100 Series Hybrid Video Recorder.

Issue

What hard drive upgrade/replacement options are available for DX8100 Series Hybrid Video Recorder?

Product Line

Pelco Video Management

Environment

DX8100

Cause

Upgrade/replacement options for storage on a DX8100.

Resolution

Hard drive upgrade and external storage expansion options  listed on page 6 of the DX8100 Specification Sheet. are now obsolete.
A total of four hard drives can be installed in a DX8100 Series. DX8100 supports up to 8TB internal storage. Hard drives larger than 2TB are not officially supported.

Current hard drive part numbers as of 4/19/16

  • EE08-3250-6206G   250GB sata hard drive. (Cannot be sold direct has to be purchase through service and repair department).
  • EE08-3500-6203G   500GB sata hard drive. (Cannot be sold direct has to be purchased through service and repair department).
  • EE11-0001-2113      1TB sata hard drive.
  • EE11-0002-2112      2TB sata hard drive.

Related Articles:

How to add and configure an additional storage Hard Drive to a DX8100?