What are the default login credentials for Endura Utilities?

Issue

What are the default login credentials for Endura Utilities?

Product Line

Pelco Video Management

Environment

Endura Utilities

Cause

Default username and password to log in to the Endura Utilities.

Resolution

In older versions of Endura Utilities (2.2 or older), the username "Administrator" is already populated into the "username" field. For these versions, the default password for Endura Utilities is configapp.

In all new releases (2.3 and newer), the username and password fields are initially empty, allowing users to log in with their Endura Credentials, the default of which is username: admin, password: admin. Any user assigned to an Administrative role created within Endura WS5000/5200 setup may be used.  If non-administrative credentials are used then an error message will be generated and Endura Utilities functions will be limited.  See screenshot below.