How many concurrent users does the DX4500/DX4600/DX4700/DX4800 Series DVR/HVR support?

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

How many concurrent users/connections does the DX4500/DX4600/DX4700/DX4800 Series DVR/HVR support?

Product Line

Pelco Video Management

Environment

  • DX4500/DX4600 DVR
  • DX4700/DX4800 (HD)
  • DX4100 Series
  • DX4500/DX4600 Client
  • DX Series Client
  • DS ControlPoint

Cause

Installation - Multiple viewers or connections

Resolution

  • The DX4500/DX4600 Series DVR/HVR supports 5 concurrent users logged into any system simultaneously.  Allows 2 Power User (includes single Administrator) and 3 Standard User accounts to be logged in simultaneously.
     
  • The DX4700/DX4800 Series HVR supports 5 concurrent users logged into the system simultaneously, allows multiple logins using the same username.
     

Related articles:

Can a normal user on the DX4500/DX4600 review recorded video?