Is it possible to use one WS5200 user interface to view and playback video from multiple EnduraXpress EE500 network video recorders (NVRs)?

Issue

Is it possible to use one WS5200 user interface to view and playback video from multiple EnduraXpress EE500 network video recorders (NVRs)?

Product Line

Pelco Video Management

Environment

  • Endura EE500- All versions
  • Endura WS5000- All versions

Cause

Information on the capability of the WS5000 software to connect to multiple EE500 systems simultaneously is needed.

Resolution

No, the WS5200 software must be running on a network with only one EE500. However, up to 32 WS5200 user interfaces can connect simultaneously to one EE500.