What devices are required to view megapixel cameras on the Endura System from a CM9700 System?

Issue

What devices are required to view megapixel cameras on the Endura System from a CM9700 System?

Product Line

Pelco Video Management

Environment

Endura UDI5000-MTRX- All versions

Cause

Information regarding devices needed to view Endura megapixel cameras is desired.

Resolution

In Matrix Digital Decoder Mode, the UDI5000-MTRX bridges Endura products to the CM9700 Series matrix system (using 9.03.012 software or later versions). Adding the UDI5000-MTRX with a NET5402R-HD to a matrix system allows security professionals to leverage the digital advantages of Endura with their tried and true CM9700 Series matrix system. This allows users to continue viewing live analog video through the matrix while viewing digital live or recorded video from the Endura system through the NET5402R-HD high definition digital decoder. Thus, the UDI5000-MTRX allows facility and property managers to continue leveraging the investments made in the analog matrix switch and operator training while taking full advantage of today's IP and megapixel cameras.

The following Endura devices and accessories are required to integrate the two systems:

Endura Devices:
To purchase these items, contact Pelco Sales.

     1 x UDI5000-MTRX (In Matrix Decoder Mode)
­     1 x NET5202R-HD Decoder
     
Accessories:
To purchase these items, contact the vendors provided:

     1 x Lantronix UDS1100 IP to serial converter (Lantronix.com
­     1 x DB25 (male) to DB 9 (female) cable
­     1 x RS232 to RS422 adapter
­     ­1 x Gefen Scaler - part# GTV-HDMI-2-COMPSVID (Gefen.com)
­     1 x HDMI to DVI adapter – part# ADA-DVIM-2-HDMIF (Gefen.com)
­     1 x DVI to DVI cable (Comes with the Gefen Scaler)
­     1 x RCA cables with RCA to coaxial adapter