Is it possible to install the BB53T-PG Spectra III Series back box in an outdoor environment?

Issue

Is it possible to install the BB53T-PG Spectra III Series back box in an outdoor environment?

Product Line

Pelco Cameras

Environment

  • BB53-PG
  • BB53T-PG
  • BB4-PG

Cause

To determine if Spectra series is indoor or outdoor model.

Resolution

No. The correct Spectra III back box for an outdoor application is the BB53T-PG-E. The letter "E" designates ENVIRONMENTAL model that includes the heaters and blowers with Sun Shroud.