I need to remove the TXB Series Translator Board from the Esprit, what do I need to replace it with? How do I test a PTZ camera using a Pelco Fiber transmitter board?

Issue

I need to remove the TXB Series Translator Board from the Esprit, what do I need to replace it with?

Product Line

Pelco Cameras

Environment

  • Spectra IV
  • TXB-HEADER
  • TXB Cards
  • FS Fiber Modules

Cause

Removal of TXB protocol or TXB IP encoder card. Jumper block required to return video and control as an analog system.

Resolution

When the TXB Translator Board; Encoder; or Fiber module is removed, you will need to replace it with the TXB-HEADER.

See Lessons Learned Article #12255 for view of TXB-HEADER.