What is the network connection speed requirement for IP cameras and single channel Endura Encoders when connecting to an Endura System?

Issue

What is the network connection speed requirement for IP cameras and single channel Endura Encoders when connecting to an Endura System?

Product Line

Pelco Video Management

Environment

  • Endura NET5301T- All versions
  • Endura NET5401T- All versions
  • All Pelco IP cameras- All versions

Cause

Information regarding the connection speed needed between an IP camera/encoder and the Endura System.

Resolution

IP cameras and single channel Endura Encoders require a 100Mbps network connection when connected to an Endura System.