Issue
Which dip switch on Spectra IV should be ON when using Coaxitron control with third party devices or CM9700 Systems and CM9760-CXTA?
Product Line
Pelco Cameras
Environment
Spectra IV version 1.070 or newer
Third-party PTZ control device
CM9700 System with CM9760-CXTA
Cause
Dip switch 2 number 3 (SW2 #3) was OFF
Resolution
SW2 #3 should be ON when using Coaxitron control with a third party device.