What product is required to mount the SD435-PG-E0 Spectra Pendant Series to a pole?

Issue

What product is required to mount the SD435-PG-E0 Spectra Pendant Series to a pole?

Product Line

Pelco Cameras

Environment

  • Spectra Pendant Series
  • Spectra Heavy Duty Series
  • IWM-GY or IWM24-GY Series
  • PA402

Cause

Options for mounting of Spectra Series to a round pole.

Resolution

Mounting the Spectra Pendant Series to a round pole requires the following optional product:

  • IWM-GY wall mount or IWM24-GY
     
  • PA402 pole adaptor