What version Pelco System Manager is compatible with CM9700-CC1 executable version 9.03.0xx?

Issue

What version Pelco System Manager version is compatible with CM9700-CC1 executable version 903.045 and higher?

Product Line

Pelco Matrix

Environment

  • CM9760-CC1 CPU controller
  • CM9700-CC1 CPU controller

Cause

Programming software versions must match the executable versions of the CM97xx CPU controlled otherwise corruption of the system files will occur.

Resolution

For CM9700-CC1 executable version 9.03.045 and higher use Pelco System Manager version 9.03.032.