What is the hard drive type and size for the DX8000 Series DVR.

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

What is the hard drive type and size for the DX8000 Series DVR.

Product Line

Pelco Video Management

Environment

  • DX8000 Series DVR
  • Hard drives

Cause

Replace failed hard drive.

Resolution

Type = IDE Seagate or Western Digital hard drive and 7200 RPM speed.
Size = 250 GB (max) per drive

Note:

  • Maximum hard drive size on DX8000 DVR  is 250GB X 4 = 1000GB (1TB)
  • If using any manufacture hard drive other than Maxtor you will need to install the Intel Application Accelerator patch.