Is there a way to export configuration settings from a DX7100 to a DX8100?

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

Is there a way to export configuration settings from a DX7100 to a DX8100?

Product Line

Pelco Video Management

Environment

  • DX7100 Series DVR
  • DX8100 Series HVR

Cause

Keep the current DX7100 configuration by importing the DX7100 configuration file to DX8100 Series HVR.

Resolution

The DX7100 configuration import/export works only with the DX7100 Series DVR's. 
The DX8100 Series HVR also has a configuration import/export option which also works with the DX8100 Series HVR's only.


For more information on the DX8100 configuration import/export, please see the DX8100 Series Upgrade and Recovery Manual, page 4.