Telescoping pendant pole mount for the pendant Sarix IE cameras

Issue

Is the telescoping pendant pole mount for the pendant series IE cameras?

Product Line

Pelco Cameras

Environment

  • Sarix Domes with 1.5 NPT threading

Cause

Option to mount Sarix Domes from a ceiling telescoping pole.

Resolution

Part Number  SP99-321 is for use with Pendant Domes that use 1.5-Inch NPT Pipe.

  • Mounts to MRCA Ceiling Adapter
  • Click Here for view of Specification Sheet.