RS422 parity for a CM9760-CXTA Coaxitron Translator

Issue

What is the RS422 parity for a CM9760-CXTA Coaxitron Translator?

Product Line

Pelco Cameras

Environment

  • CM9760-CXTA
  • RS422 Control System

Cause

Programming, Switch Setting or Fixed settings of Parity protocol for matching

Resolution

When to operating in P protocol the CM9760-CXTA will be set for EVEN parity. In D protocol the CM9760-CXTA requires RS422 communications at 2400 baud with NO parity.