How many simultaneous remote connections can a single DX8000/DX8100 Series recorder accept?

Issue

How many simultaneous remote connections can a single DX8000/DX8100 Series recorder accept?

Product Line

Pelco Video Management

Environment

  • DX8000 Series
  • DX8100 Series
  • DX8000 Client
  • DX8100 Client
  • DX Series Client
  • DS ControlPoint

Cause

Multiple users require viewing.

Resolution

The DX8000/DX8100 will allow 5 maximum users at one time.

Note:

  • The limit includes Server to Server, Client to Server and Web Client to Server concurrent connections.
  • DX Series DVRs does not allows the same user account to login multiple times from different locations including the DVR.


Example: If the admin user is currently login at the DX8100/Dx8000 DVR, the admin user cannot login from the client PC. A different user
account needs to be used or log-out the admin user from the DVR to be able to use it at the client PC.