Spectra Display Setup

Issue

How can I turn off the time/date display on Spectra cameras?

How can I turn off the Azimuth and Elevation display on Spectra cameras?

Product Line

Pelco Cameras

Environment

  • Spectra IV / IVse Series
  • Spectra III Series

Cause

Configuration - Navigate the Spectra menu.

Resolution

  1. From the operator keyboard display the camera on a local monitor.
  2. Enter the camera onscreen menus by selecting 95 Preset.
  3. Using the keyboard joystick or direction keys, navigate to Display Setup and press iris open.
  4. Navigate to desired itemand press iris open.
  5. Toggle the setting to OFF and press iris open.
  6. Navigate to Exit and press iris open to exit the menu.