How to program a pattern on a KBD300A keyboard

Issue

How to program a pattern on a KBD300A keyboard

Product Line

Pelco Video Management

Environment

  • KBD300A keyboard

Cause

Create an unique PTZ (Pan Tilt Zoom) pattern for the camera to follow when the pattern is called.

Resolution

Program a pattern

  1. With the SHIFT LED off (not lit), press and release a number (this is the pattern number).
  2. Press and hold PATTERN for two seconds to start the pattern recording mode.
  3. Perform the desire pattern.
  4. With the SHIFT LED off (not lit), press the ACK key to stop the pattern recording mode.