Can the CM9760-KBD or KBD300A keyboard be used with the CM9760-SAT?

Issue

Can the CM9760-KBD or KBD300A keyboard be used with the CM9760-SAT?

Product Line

Pelco Matrix

Environment

  • CM9760-KBD
  • KBD300A
  • CM9760-SAT

Cause

Desktop keyboard option for the CM9760-SAT.

Resolution

The KBD300A can connect directly to the CM9760-SAT, the CM9760-KBD is not compatible with the CM9760-SAT.