Will a power supply rated at 12 volts 1 amp work with the CM9760-DMR?

Issue

Will a power supply rated at 12 volts 1 amp work with the CM9760-DMR?

Product Line

Pelco Matrix

Environment

CM9760-DMR Data Manager

Cause

Missing power supply

Resolution

Yes. This will work although the CM9760-DMR originally shipped with a power supply that is rated at 9 volts.