Power connector in the back box of the Spectra IV Series dome drive

Issue

Where do you connect the power wires in the back box of the Spectra IV Series dome drive?

Product Line

Pelco Cameras

Environment

Spectra IV Series

Cause

Location to install the power wires on the back box board is unknown.

Resolution

Connect the 24 VAC to the PWR + and PWR- terminals in the back box of the Spectra IV Series dome drive. Refer to the image below for the location of the power connector.