Program a pattern on the Spectra III Series dome

Issue

Can you program a pattern from the menu of the Spectra III Series dome?

Product Line

Pelco Cameras

Environment

Spectra III

Cause

Navigate to dome settings to program a pattern.

Resolution

Yes you can you program a pattern from the menu of the Spectra III Series dome.

  1. Enter the preset 95 menu
  2. Select dome settings and press  iris open
  3. Select patterns press  iris open
  4. Select program pattern and press  iris open
  5. Move the dome to the starting position and press  iris open to begin the pattern.
  6. Move the dome through its pattern and press  iris open to store the pattern.
  7. Exit the menu