How often does the SM5000 communicate with the other Endura devices?

Issue

How often does the SM5000 communicate with the other Endura devices?

Product Line

Pelco Video Management

Environment

Endura SM5000- All versions

Cause

There is a need to adjust the intervals for SM communications.

Resolution

There are two things to take into account when estimating SM communications, Device Startup Interval and Device Renewal Interval.

Device startup interval: 
This defines how long the network devices will wait before advertising their presence on the network during system startup. The default setting is 60 seconds.
 
Device renewal interval: 
This defines how often the network devices advertise their presence on the network during normal operations. The default setting is 1800 seconds (30 minutes)