Can I connect two NET5300B base encoders to one CM9760-CDU-T?

Issue

Can I connect two NET5300B base encoders to one CM9760-CDU-T?

Product Line

Pelco Transmission & Power

Environment

  • NET5300B
  • CM9760-CDU-T

Cause

Merge two NET5300B encoders to one CM9760-CDU-T for code distribution.

Resolution

This application require the addition of one CM9760-DMR in merger mode. 

Please r
efer to the CM9760-DMR Installation and Operation Manual