Issue
What address is used for Coaxitron control on the Spectra IV Series dome drive?
Product Line
Pelco Cameras
Environment
Spectra IV (analog series)
Cause
Switch settings for selecting coaxitron control.
Resolution
The Spectra IV Series dome drive auto senses the Coaxitron signal. An address setting is not required. Default dip switch settings will be overridden when PTZ commands are given from head end controller.
- Click Here for Pelco knowledgebase article titled 'What switch should I turn on to make the Spectra IV work with Coaxitron and third party fiber?'
- Click Here for Pelco knowledgebase article titled 'Dip Switch settings on the Spectra IV when using Coaxitron protocol with third party control devices.'