Adjust the IR cut filter on the Spectra III or IV Series dome drive.

Issue

Adjust for color, or black and white video.

Product Line

Pelco Cameras

Environment

  • Spectra III Series
  • Spectra IV Series
  • KBD300A

Cause

  • Installation

Resolution

For Spectra III Series
 
  1. Enter the preset 95 camera menu.
  2. Joystick to Dome settings and press Iris Open.
  3. Joystick to Camera and press Iris Open.
  4. Joystick to IR Cut Filter and press Iris Open.
  5. Joystick up or down to change between Auto, In, Out, or Manual and press Iris Open.
  6. Joystick to exit and press Iris Open.

     
For Spectra IV Series
 
  1. Enter the preset 95 camera menu.
  2. Joystick to Dome Settings and press Iris Open.
  3. Joystick to Camera IR Cut Filter and press Iris Open.
  4. Joystick up or down and highlight Auto, in, Out, or Manual and press Iris Open.
  5. Joystick to exit and press Iris Open.