Star Configuration or Home Run of multiple Spectra, Esprit, Exsite cameras to single controller

Issue

How do you Star Configuration ( Home Run ) multiple Spectra cameras to a single KBD300A Keyboard?

Product Line

Pelco Cameras

Environment

  • Spectra Series
  • Esprit Device
  • Control End Device
  • Two - Wire Control

Cause

  • Spectra or Esprit cameras installed at various locations of site. Installation locations of PTZ cameras does not allow for daisy chain of data.
  • No or Sporadic Pan Tilt control of Spectra or Esprit cameras.

Resolution

Daisy-chaining (going from one receiver to another) is recommended but not always possible. A maximum of 16 receivers can be daisy chained from a controller port.

If more that 16 receivers are required for your system, or if you do not want to daisy-chain the receiver connections, use the CM9760-CDU-T.

Click Here to view a wiring diagram of Spectra to CM9760-CDU-T

 

NOTE: Communication is RS-422. Maximum cable distance for RS-422 communication over 24-gauge wire is 4000 feet (1,219 m). Pelco recommends using shielded twisted pair cable that meets or exceeds the basic requirements for EIS RS-422 applications.