What are the inside and outside diameter of the PP350, PP450 pipe?

Issue

What are the inside and outside diameter of the PP350, PP450 pipe?

Product Line

Pelco Cameras

Environment

  • PP350
  • PP450

Cause

Dimensions of Parapet Pipe diameter

Resolution

Outside diameter of the PP Series tube is 2.500" (0.0635 m)

Inside diameter of the PP Series tube is 2.250" (0.05715 m)