Where is the 3 amp fuse for the WCS4-20B located?

Issue

Where is the 3 amp fuse for the WCS4-20B located?

Product Line

Pelco Transmission & Power

Environment

WCS4-20B power supply

Cause

Outputs on the WCS4-20B does not power up the outdoor units.

Resolution

The B series models do not require a fuse, it uses circuit breakers. The WCS4-20B outdoor power supply protected outputs with self-resetting circuit breakers and will self-reset when the fault is corrected.