Where can I download the latest version of Digital Sentry software?

Issue

Would like to install the most recent version of Digital Sentry software available.

Product Line

Pelco Video Management

Environment

  • Digital Sentry
  • DSSRV / DSSRV2
  • DSNVS

Cause

Would like to download the latest version of Digital Sentry software.

Resolution

www.pelco.com

  • Digital Sentry SRV (version 7.18) download: DSSRV Page
  • Digital Sentry NVs (version 7.18) download: DS NVs Page
     

Note: The DSInstaller is for Digital Sentry software running on Pelco hardware.  The NVSInstaller is for the software only solution running on customer hardware.


As of Digital Sentry software version 7.7.309 and above, Microsoft .NET 4.5.1 is required which means Windows XP and Windows 2003 Server are no longer supported.   The DS 7.7.309 installer package does not include .NET 4.5.1, if .NET 4.5.1 is not preinstalled on the server the installer will initiate a download of .NET 4.5.1 from microsoft which will require Internet access.    If there is no Internet access at the server location and .NET 4.5.1 is not preinstalled, download a standalone installer here : http://www.microsoft.com/en-us/download/details.aspx?id=40779

Related Articles:
How to install the Digital Sentry Software Suite on Digital Sentry HVR(s) and NVR(s).