NET5500 Accessory Packs

Issue

What is the part #'s for the accessory packs for the NET5500 series encoders?

Product Line

TAC I/NET, Other

Environment

NET5501

NET5501-XT

NET5504

NET5508

NET5516

Cause

No part #'s listed in BOM, specification sheets or manuals for the accessory pack.

Resolution

The below part's are the accessory packs that come with each type of NET5500 series encoder:

1.  NET5501-I accessory pack part # ZSPNET5500-10

2.  NET5501-XT accessory pack part # ZSPNET5500-11

3.  NET5501 accessory pack part # ZSPNET5500-0012

4.  NET5504 accessory pack part # ZSPNET5500-0013

5.  NET5508 accessory pack part # ZSPNET5500-0014

6.  NET5516 accessory pack part # ZSPNET5500-0015

 

 

 

Accessory pack includes: