How to connect to an Oncam Evolution 360 Media stream (EVO-05 & EVO-12).

Issue

Need to connect to an Oncam Evolution 360 Media Stream.

Product Line

Pelco Video Management

Environment

EVO-05 Firmware version 1.9.18

EVO-12 Firmware version 1.4.96

Cause

Need to connect to the Oncam Evolution Media Stream.

Resolution

 
H.264 video stream - EVOLUTION-05
 
4MP H.264 video stream : rtsp://(camera_ip_address)/h264/video.sdp?camera=13
 
2MP H.264 video stream : rtsp://(camera_ip_address)/h264/video.sdp?camera=25
 
1MP H.264 video stream : rtsp://(camera_ip_address)/h264/video.sdp?camera=12
 
¼ H.264 video stream : rtsp://(camera_ip_address)/h264/video.sdp?camera=26
 
 
For Example, to view an H.264 stream in Evolution camera with an IP address of 192.168.1.100 and stream = 4MP H.264 will be;
 
rtsp://192.168.1.100/h264/video.sdp?camera=13
 
 

 
H.264 video stream (Multicast) - EVOLUTION-05
 
rtsp://admin:admin@(camera_ip_address):8556/h264/multicast.sdp
 
 
For Example, to view an H.264 multicast stream in Evolution camera with an IP address of 192.168.1.100 will be;
 
rtsp://admin:admin@192.168.1.100:8556/h264/multicast.sdp
 
 

 
MJPEG video stream - EVOLUTION-05
 
 
4MP MJPEG video stream :http://(camera_ip_address:port_number)/video.cgi?camera=13
 
2MP MJPEG video stream : http://(camera_ip_address:port_number)/video.cgi?camera=25
 
1MP MJPEG video stream : http://(camera_ip_address:port_number)/video.cgi?camera=12
 
¼ MJPEG video stream : http://(camera_ip_address:port_number)/video.cgi?caera=26
 

 
Media Stream - EVOLUTION-12
 
 
Fisheye 1: rtsp://(camera_ip_address)/video.sdp?name=FE1
 
Fisheye 2: rtsp://(camera_ip_address)/video.sdp?name=FE2
 
Vcam 1: rtsp://(camera_ip_address)/video.sdp?name=VC1
 
Vcam 2: rtsp://(camera_ip_address)/video.sdp?name=VC2
 
Vcam 3: rtsp://(camera_ip_address)/video.sdp?name=VC3
 
Vcam 4: rtsp://(camera_ip_address)/video.sdp?name=VC4