Oncam Evolution camera does not support multicast when using ONVIF (EVO-05 & EVO-12)

Issue

If you have a VxS configured to record multicast and you add an EVO-05 or EVO-12 camera, it will only record unicast, not multicast.

Product Line

Pelco Video Management

Environment

EVO-05 Firmware version 1.9.18

EVO-12 Firmware version 1.4.96

Cause

You configure your VxS to record multicast, but instead end up recording unicast when using the ONVIF driver with your evolution camera.

Resolution

Oncam Evolution camera does not support multicast when using ONVIF (EVO-05 & EVO-12)