Full logic syntax is supported. By default, all search terms are included in the search. Use the | symbol or type "OR" to find either of two search terms. A dash or hyphen directly before a term will return only articles without that word. Quotation marks around a series of words will search for that exact phrase.
Example: "xenta server" (511|527) -firmware