Issue
Unable to launch WebPinpoint graphics on client machines and/or at the webserver. Receiving the following errors when trying to launch a graphic in WebClient
- Could not connect to server. Cause: The remote server returned an error: (404) Not Found
- Could not create ACWPPServerProxy Application on the remote server.
- Server: http://0.0.0.0/DNWACServerFactory/WACServerFactory.soap.
Environment
IIS
WebClient
WebPinpoint
Cause
In IIS, the DNWACServerFactory authentication was failing when configured for Passthrough authentication.
Resolution
- Deselect Passthrough Authentification. (In Windows 7 you'll find this in IIS under DNWACServerFactory Basic Settings.
- Use Windows Authentication
- Enter the Windows User and Password. The connection should succeed.
- Reboot the IIS Server
- The accwppserverproxy process stays up and graphics launch properly.