Issue
How to Logon / Logoff Continuum using a button on a Graphic or Menu page.
Environment
Continuum Cyberstation
Cause
Want to be able to Logon Continuum with the click of a button from Graphics or Menu page and also bring up the Logon prompt the same way.
Resolution
** DISCLAIMER ** This application is not a supported part of Continuum and is provided as-is.
1. Copy the "Logoff.tx_" file in this archive, here, to the Continuum folder (c:\Program Files\Continuum).
2. Rename the .tx_ file extension to .exe.
3. Create hotspots / buttons as below to call the program with the two available command line arguments; 1 will logon, 2 will logoff.
Suggested usage:
On the Main Continuum Menu page create two buttons, one for logon, one for logoff. (Pinpoint could also be used for Logoff but would not work for Logging back on - Pinpoint closes when the user is logged off.)
For the Logon Button:
Set control to: Execute
Open: C:\ProgramFiles\Continuum\Logoff.exe
Arguments: 1
Button Text: Logon
For Logoff Button:
Set control to: Execute
Open: C:\ProgramFiles\Continuum\Logoff.exe
Arguments: 2
Button Text: Logoff