Issue
A TGML Graphic is added or imported into Vista. Then when you right click on the TGML Graphic and select " Open Bindings Window" a blank bindings window is opened.
None of the objects defined in the TGML Graphic appear in the binding list to be bound to objects in the Vista database.
Environment
Vista 5.1.7
Cause
The TGML Graphic is named with .(dot) characters in the name. E.G. VAV1.1.7
Resolution
Do not use dots, dashes or hyphens in the naming convention for any Vista objects. Either eliminate it altogether, or use underscores (_) instead.
To correct this issue after the TGML Graphic has been added with the incorrect naming convention, is:
- Edit the TGML Graphic and save it out of the database.
- Delete the TGML Graphic with the name including the . (dot) character.
- Add a new TGML Graphic using the correct naming convention E.G. VAV1_1_7
- Open the TGML Graphic that was saved out of the database and save into the new TGML Graphic you created with the correct naming convention.
Note: Renaming the TGML Graphic object from VAV1.1.7 to VAV1_1_7 in the Vista database does not fix the problem.