BACnet IP port supported with StruxureWare Building Operation

Issue

BACnet IP port supported with StruxureWare Building Operation

Product Line

SmartStruxure Solution

Environment

BACnet interface in a StruxureWare Building Operation site either with the ES or AS

Cause

What BACnet IP ports are supported with StruxureWare Building Operation and can there be more than one port?

Resolution

StruxureWare Building Operation does support 47808 by default and this adjustable to higher or lower. StruxureWare Building Operation only supports a single value, in other words, it cannot be more than one single port.

Please note that BacNet IP use UDP as its transmission protocol. For more information read the BACnet/IP basic design criteria.